VDRB05981-03

Replacement of Components and Cubicles

The drive mechanisms, current transformers and voltage transformers as well as the testing and monitoring systems can be replaced if necessary Also, entire panels can be replaced.

For any queries regarding replacement of components or panels, please contact Schneider Electric.

The data on the nameplate are relevant for replacement of components or panels or in case of any queries. Refer to Nameplate.


NOTE: PT fuse, LV control fuse, SMPS, Battery, Power pack, Surge arrestor, LLI, VPIS, FPI, battery, Relay battery, Relay memory card, and Battery charger is a consumable parts. It is not covered by free replacement, even though the product is under the warranty period.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?