VDRB05981-03

Transport of the Cubicles and VCB on the Construction Site

WARNING
HAZARD of toppling
  • Ensure the ropes or chains are strong enough to bear the weight of the cubicle and the trucks.
  • Comply with the relevant provisions for hoisting equipment.
  • When lowering the cubicles and trucks, ensure that the supporting platform is stable and level.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
HAZARD of FALLING
Watch out for floor openings in the switchgear room.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?