VDRB05981-03

Access to the Cable Compartment

DANGER
hazard of electric shock, explosion, or arc flash
Before accessing the cable compartment, ensure the following
  • Earth Switch is ON.
  • EvoPacT HVX-O VCB is OFF and in disconnected/test condition.
  • Check the VDIS indication for zero voltage across the cubicle.
Failure to follow these instructions will result in death or serious injury.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?