High-voltage Connection
Cable Connection Variants Overview
|
In Cubicle (A) |
Panel width (mm) |
Cables per Phase |
|---|---|---|
|
800 |
1000 |
1/2 |
|
1250 |
1000 |
1/2/3/4 |
|
2000 |
1000 |
4/5 |
|
2500 |
1000 |
5/6 |
|
3150 |
1000 |
6 |
Installing the High-voltage Cables
Screws, bolts, and plastic plates are provided to assemble the clamping for high-voltage cables. Refer to Access to the Cable Compartment.
Preparation of the Cable Compartment
-
Remove the cable clamp fasteners.
-
Drill the cable plastic plate as per cable requirement.
-
Remove the plain gland plates and drill as per cable requirement.
|
1 |
Cable clamps |
3 |
Plastic plates |
|
2 |
Cable clamp fasteners |
4 |
Plain gland plates |