VDRB05981-03

Operation Accessories

NOTICE
hazard of inadequate use conditions
Ensure to operate the panel using only the accessories supplied with it.
Failure to follow these instructions can result in equipment damage.

List of Operational Accessories

Description

Item number

Illustration

Standard double-bit key to lock/unlock the door of the LV cabinet.

SEM101137–01

Crank to charge the CB’s energy storing device

MVIA00207–01

Operating rod to switch the CB ON and OFF

MVIB00775–01

Truck handle (rack-in/rack-out)

VDRG00157–04

Operating lever for the earthing switch

VDRB05405–01

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?