VDRB05981-03

Applicable Standards and Regulations

The applicable standards and regulations are as follows:

  • Metal-enclosed; loss of service continuity category according to IEC 62271-200: LSC 2B-PM.

  • Type-tested.

  • Tested for internal faults (qualification IAC AFLR).

Applicable Standards and Regulations for PIX-36 Cubicles

Designation

IEC Standard

EN Standard

Switchgear

IEC 62271-200

IEC 62271-200

IEC 62271-1

IEC 62271-1

Internal Arc Classification (IAC)

IEC 62271-200

IEC 62271-200

Circuit Breaker

IEC 62271-100

IEC 62271-100

Earthing Switch

IEC 62271-102

IEC 62271-102

Current Transformer

IEC 60044-1

IEC 60044-1

Voltage Transformer

IEC 60044-2

IEC 60044-2

Voltage Detecting Systems

IEC 61243-5

IEC 61243-5

IEC 61958

IEC 61958

Protection against accidental contact, foreign bodies and water

IEC 60529

IEC 60529

Degree of protection against accidental contact, and foreign objects according to IEC 62271-200 and IEC 60529

Description

IPX Rating

Degree of protection of the switchgear enclosure

IP4X

Degree of protection of the accessible claddings in the cubicle

IP2X

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?