VDRB05981-03

Cleaning

DANGER
HAZARD OF ELECTRICAL ARC, EXPLOSION AND FIRE
  • To maintain the cubicle insulating level , ensure that the insulating components are clean.
  • Wear appropriate PPE before any cleaning operation.
  • Only use the cleaning agent specified by Schneider Electric (reference no. S008152).
  • Check the cubicle for any dirt buildup.
  • Clean the contaminated components with a dry, clean, and lint free cloth.
  • Depending on the level of soiling, replace the cloth as required.
  • Soak the cloth thoroughly in a recommended cleaning agent and wipe the insulating components.
  • Keep the duration of exposure as short as possible.
  • Expose the cleaned surface to air at least for two hours.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?