VDRB05981-03

Switching the EvoPacT HVX-O VCB Electrically

Switching ON (Closing)

Actuate closing release via bay computer or remote control.

The energy storing device can be charged immediately after switching ON (either manually or by motor). If voltage is applied to the motor, charging is performed automatically.

Switching OFF (Opening)

  • Actuate the opening release via the bay computer or the remote control

  • By under voltage release or

  • By secondary release.

Position indicators on circuit-breaker and possible operating sequences

Item

Position indicator Energy-storing device (closing spring)

Position indicator ON/OFF Switch position

Possible operating sequence

1

Released

OFF

None

2

Charged

OFF

C–O

3

Released

ON

O

4

Charged

ON

O–C–O

C = Switching ON (Closing)

O = Switching OFF (Opening)

 
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?