Safety Provisions
Before performing work on the cubicle, it is essential that you comply with the following instructions:
DANGER |
|---|
|
HAZARD OF electric shock, explosion, or arc flash
Before removing covers and performing assembly or maintenance
work:
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
HAZARD OF MOVABLE PARTS IN MECHANICAL DRIVES
Before performing mounting and maintenance work, comply
with the below safety rules:
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING |
|---|
|
HAZARD OF SHARP-EDGED SHEET METAL AND METAL PARTS
During installation and maintenance work, comply with
the below safety rules:
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
CAUTION |
|---|
|
HAZARD OF INAPPROPRIATE HANDLING, STORAGE AND INSTALLATION
Failure to follow these instructions can result in injury or equipment damage.
|
Behavior in Case of Incidents or Accidents
If an internal arc fault occurs, the PIX-36 switchgear is equipped with pressure relief absorbers or ports to help prevent the cubicles and switchgear from being blown off.
This user and maintenance guide does not include information regarding the safety of buildings in case of internal faults (pressure load of the switchgear room and necessary pressure relief ports). Pressure calculations for switchgear rooms, including recommendations for pressure relief ports, are available upon request for a fee. For more details, contact Schneider Electric.
In case of fire or internal faults, toxic and caustic decomposition products are produced. Comply with the locally applicable accident and safety provisions.
Make sure that the first-aid measures are taken in case of injury to persons.
DANGER
WARNING
CAUTION