VDRB05981-03

Access to Main Circuit Compartment

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Ensure that the truck is in disconnected/test position before opening the front door.
  • Turn off all power supply or de-energize the complete panel because opening any door is not allowed if the busbar or cable is live.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?