VDRB05981-03

Packaging

NOTICE
Hazard of incorrect handling
  • Competent operators must handle the lifting of the cubicle.
  • It is recommended to use inspected cranes or forklifts for transportation.
  • The lifting or handling of the cubicle from the loaded transportation vehicle should be done safely.
  • Careful disassembly of the packaging is essential to help prevent damage to the cubicle.
Failure to follow these instructions can result in equipment damage.

The packaging for various modes of transportation are as follows:

  • If packed exclusively for truck transport, the cubicles are delivered on a pallet with PE protective film.

  • For sea transport, the units are packed in sealed aluminium foil with desiccant and in a closed wooden case with tightly closed wooden base (also for container transport.

  • In case of air transport, the cubicles are packed in wooden crates with a protective PE film hood (dust protection) or in wooden crates, also with closed wooden bases, however without protective hoods.

NOTE: Observe the centre of gravity label to help ensure safe transport. You can find the label on the packaging and on the switchgear cubicle.

Packed in PE protective Film on a pallet

Packed in PE protective film suitable for seaworthy transport

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?