VDRB05981-03

Environmental and Operating Conditions

PIX-36 is an indoor switchgear and may only be operated under normal conditions in accordance with IEC 62271-1.

Operation under conditions deviating from these is only admissible subject to consultation with and written approval from the manufacturer.

Ambient Conditions Accordance to IEC 62271-1

Description

Values

Temperature class

-5 °C, indoor(1)

Ambient temperature minimum/maximum

-5 °C/ +40 °C(1)

Average value over 24 hours

= 35 °C(1)

Mean relative air humidity: 24 hours/1month

≤ 95%/≤ 90%

Installation altitude above sea level

≤ 1000 m

(1) Other values are available on request.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?