VDRB05981-03

Transport of the Cubicle on the Floor

WARNING
hazard of storing under inadequate conditions
Ensure sufficient stability and evenness of the supporting area (floor).
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Follow the below steps to move the panel on the floor:

  1. Use three rollers with a minimum diameter of 30 mm.

  2. Move the panel on the rollers to its final site of installation.

Transport of the Cubicle on the Floor

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?