VDRB05981-03

Move the Truck into Service/Disconnected Position

The truck can only be moved into connected/service or disconnected/test position when de-energized.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Switch OFF the EvoPacT HVX-O VCB or, in the case of isolate the feeder.
  • Do not pull the crank out before the EvoPacT HVX-O VCB has reached its end position.
  • Do not pull the crank out in an undefined intermediate position.
Failure to follow these instructions will result in death or serious injury.

Initial Situation:

  • Circuit Breaker OFF

  • Earthing Switch OFF

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?