VDRB05981-03

Rack-out the Truck from Service Position into Disconnected Position

Follow the below steps to rack-out the truck from connected/service position to disconnected/test position:

  1. Move the slider (1) to the left and hold it.

  2. Insert truck handle (2) through the opening guide in the door onto the drive shaft of the CB truck.

  3. Turn truck handle (2) counter-clockwise until the truck is racked-out.

  4. Remove and place the truck handle back into the tool board.

  5. Check the position of the truck through the inspection glass (3).

Truck racked-out in disconnected position

Racking-out the Truck via Truck Handle


1

Slider

2

Handle

3

Indicator

NOTE: During the rack-in/rack-out, the door gets locked to help prevent it from opening. The door can be unlocked only if the truck is in the disconnected/test position.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?