Switching the EvoPacT HVX-O VCB Manually
Switching ON via the Operating Rod
The closed-door operation of the EvoPacT HVX-O VCB involves switching the EvoPacT HVX-O to the connected/service position or rack-in position.
Follow the below steps to switch ON the CB via operating rod:
-
Take the operating rod from the tool board.
-
Insert the operating rod into the guide of the front door.
-
Push the switch ON button with the operating rod.
WARNINGHAZARD OF INAPPROPRIATE OPERATIONEnsure that the EvoPacT HVX-O VCB is switched ON via operating rod and the position indicator indicates ON through the inspection glass.Failure to follow these instructions can result in death, serious injury, or equipment damage. -
Remove the operating rod from the guide of the EvoPacT HVX-O door.
-
Place the operating rod back into the tool board.
Switching OFF via the Operating Rod
Follow the below steps to switch OFF via operating rod:
-
Take the operating rod from the tool board.
-
Insert the operating rod through the guide of the circuit breaker front door.
-
Push the switch OFF button with the operating rod.
WARNINGHAZARD OF INAPPROPRIATE OPERATIONEnsure that the CB is switched OFF via push rod and the position indicator indicates OFF through the inspection glass.Failure to follow these instructions can result in death, serious injury, or equipment damage. -
Remove the operating rod from guide of CB door.
-
Place the operating rod back into the tool board.