VDRB05981-03

Switching ON the Earthing Switch

Initial Situation:

  • Earthing switch: OFF

  • Circuit Breaker: OFF

  • Truck: Disconnected position

Follow the below steps to switch ON the earthing switch:

  1. Rotate the flap anti-clockwise to access the operating shaft.

  2. Insert the operating handle aligned with axis point.

  3. Rotate the handle anti-clockwise by 90° to close the earthing switch.

  4. Check the earthing switch position indicator through cable compartment inspection window and ensure that the earthing switch is ON.

  5. Remove the operating handle and place it back into the tool board.

Operation of Earthing Switch

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?