Avatar Function Allocation
In the following table, a check mark ✔ indicates the function groups that are possible with each TeSys avatar.
Avatar Function Allocation – Protection and Monitoring
|
Name |
Current Monitoring |
Upstream Voltage Presence |
Electrical Protection |
Load Protection |
Motor Overheat Protection* |
Energy Monitoring* |
|---|---|---|---|---|---|---|
|
System avatar |
— |
— |
— |
— |
— |
✔ |
|
Switch |
✔ |
✔ |
✔ |
— |
— |
— |
|
Switch - SIL Stop, W. Cat 1/2* |
✔ |
✔ |
✔ |
— |
— |
— |
|
Switch - SIL Stop, W. Cat 3/4* |
✔ |
✔ |
✔ |
— |
— |
— |
|
Digital I/O |
— |
— |
— |
— |
— |
— |
|
Analog I/O |
— |
— |
— |
— |
— |
— |
|
Power Interface without IO (measure) |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Power Interface with IO (control) |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor One Direction |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor One Direction - SIL Stop, W. Cat 1/2 |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor One Direction - SIL Stop, W. Cat 3/4 |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor Two Directions |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor Two Directions - SIL Stop, W. Cat 1/2 |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor Two Directions - SIL Stop, W. Cat 3/4 |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor Y/D One Direction |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor Y/D Two Directions |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor Two Speeds |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor Two Speeds - SIL Stop, W. Cat 1/2 |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor Two Speeds - SIL Stop, W. Cat 3/4 |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor Two Speeds Two Directions |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor Two Speeds Two Directions - SIL Stop, W. Cat 1/2 |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Motor Two Speeds Two Directions - SIL Stop, W. Cat 3/4 |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Resistor |
✔ |
✔ |
✔ |
✔ |
— |
✔ |
|
Power Supply |
✔ |
✔ |
✔ |
✔ |
— |
✔ |
|
Transformer |
✔ |
✔ |
✔ |
✔ |
— |
✔ |
|
Pump |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Conveyor One Direction |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Conveyor One Direction - SIL Stop, W. Cat 1/2 |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Conveyor Two Directions |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
Conveyor Two Directions - SIL Stop, W. Cat 1/2 |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
In the following table, a check mark ✔ indicates the function groups that are possible with each TeSys avatar.
Avatar Function Allocation—Predictive Alarms, PV, and Control Modes
|
Name |
Predictive Alarms |
Process Variable Monitoring |
Configurable Control Modes |
|---|---|---|---|
|
System avatar |
— |
— |
— |
|
Switch |
— |
— |
— |
|
Switch - SIL Stop, W. Cat 1/2* |
— |
— |
— |
|
Switch - SIL Stop, W. Cat 3/4* |
— |
— |
— |
|
Digital I/O |
— |
— |
— |
|
Analog I/O |
— |
— |
— |
|
Power Interface without IO (measure) |
— |
— |
— |
|
Power Interface with IO (control) |
— |
— |
✔ |
|
Motor One Direction |
✔ |
✔ |
✔ |
|
Motor One Direction - SIL Stop, W. Cat 1/2 |
— |
— |
✔ |
|
Motor One Direction - SIL Stop, W. Cat 3/4 |
— |
— |
✔ |
|
Motor Two Directions |
✔ |
✔ |
✔ |
|
Motor Two Directions - SIL Stop, W. Cat 1/2 |
— |
— |
✔ |
|
Motor Two Directions - SIL Stop, W. Cat 3/4 |
— |
— |
✔ |
|
Motor Y/D One Direction |
✔ |
✔ |
✔ |
|
Motor Y/D Two Directions |
✔ |
✔ |
✔ |
|
Motor Two Speeds |
✔ |
✔ |
✔ |
|
Motor Two Speeds - SIL Stop, W. Cat 1/2 |
— |
— |
✔ |
|
Motor Two Speeds - SIL Stop, W. Cat 3/4 |
— |
— |
✔ |
|
Motor Two Speeds Two Directions |
✔ |
✔ |
✔ |
|
Motor Two Speeds Two Directions - SIL Stop, W. Cat 1/2 |
— |
— |
✔ |
|
Motor Two Speeds Two Directions - SIL Stop, W. Cat 3/4 |
— |
— |
✔ |
|
Resistor |
— |
— |
✔ |
|
Power Supply |
— |
— |
✔ |
|
Transformer |
— |
— |
✔ |
|
Pump |
✔ |
✔ |
✔ |
|
Conveyor One Direction |
✔ |
✔ |
✔ |
|
Conveyor One Direction - SIL Stop, W. Cat 1/2 |
✔ |
✔ |
✔ |
|
Conveyor Two Directions |
✔ |
✔ |
✔ |
|
Conveyor Two Directions - SIL Stop, W. Cat 1/2 |
✔ |
✔ |
✔ |
WARNING