DOCA0270EN-02

Micro SD Card

TeSys island bus couplers are designed with a card slot for a micro SD card. TeSys island maintains files on the micro SD card for the fast device replacement (FDR) function, as well as a software/firmware backup from the device and log files.

NOTE: Recommended micro SD card sizes for the TeSys island bus coupler are 4 GB, 8 GB, 16 GB, and 32 GB.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?