Coupling Starters
This section describes how to join adjacent starters with accessories for use in two direction, two speed, and wye-delta Avatars. Refer to the bill of materials (BOM) and the TeSys island topology to determine which starters require installation of accessories. See also Avatar Composition. Join the starters with the accessories before mounting them on DIN rail.
The accessories come packaged as kits or can be ordered individually. The kits and their components are described in the following tables.
LAD9R1 Assembly Kit for 9–38 A (Size 1 and 2) Starters
Kit Components |
Description |
LAD9R1 Assembly Kit |
---|---|---|
LAD9V5 |
Parallel link between two starters |
For installation instructions, refer to Installing the LAD9R1 Kit (9–38 A Starters). |
LAD9V6 |
Reversing link between two starters |
|
LAD9V2 |
Mechanical interlock with assembly staple |
LAD9R3 Assembly Kit for 40–65 A (Size 3) Starters
Kit Components |
Description |
LAD9R3 Assembly Kit |
---|---|---|
LA9D65A6 |
Parallel link between two starters |
For installation instructions, refer to Installing the LAD9R3 Kit (40–65 A Starters). |
LA9D65A69 |
Reversing link between two starters |
|
LAD4CM |
Mechanical interlock |
Shorting Blocks for Y/D Avatars
Reference Number |
Description |
Shorting Blocks |
---|---|---|
LAD9P3 |
Shorting block / 3P parallel link for 9–38
A (size 1 and 2) starters. |
For installation instructions, refer to Installing the LAD9P3 Shorting Block (9–38 A Starters in Y/D Avatars). |
LAD9SD3S |
Shorting block / 3P parallel link for 40–65
A (size 3) starters and a separate warning label. |
For installation instructions, refer to Installing the LAD9SD3S Shorting Block (40–65 A Starters in Y/D Avatars). |