DOCA0270EN-02

Motor Two Directions - SIL Stop, W. Cat 3/4

NOTE: Safety Integrity Level according to standard IEC 61508. Wiring Category 3 and Category 4 according to ISO 13849.

Wiring (See Legend Table below)

Accessories

Legend

A Mechanical interlock
B Parallel link
C Reversing link
F Forward
R Reverse
SS-1 SIL starter 1
SS-2 SIL starter 2
SS-3 SIL starter 3

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?