DOCA0270EN-02

System State Transition Events

TeSys island logs the following System State Transition events when there is any change in value of the System Avatar Status data:

  • Degraded Mode

  • Force Mode

  • Minor Event

  • Test Mode

  • Operational

  • Pre-Operational

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?