Connecting to TeSys island with SoMove Software
Perform the steps in the following table the first time you connect to TeSys island with a PC running SoMove software and the TeSys island DTM. SoMove software is a Microsoft® Windows®-based application using open FDT/DTM technology. SoMove contains DTMs for different devices. The TeSys island DTM enables the configuration, monitoring, control, and customization of TeSys island functions.
Connect to the TeSys island with SoMove Software
| 
                        
                         Step  | 
                     
                     
                        
                         Action  | 
                     |
|---|---|---|
| 
                        
                         1  | 
                     
                     
                        
                         Check the LED indicators on the bus coupler and verify that power is applied. Verify that the PWR LED, indicating the power supply and system status, is steady green and the MS LED, indicating bus coupler status, is flashing green.  | 
                     |
| 
                        
                         2  | 
                     
                     
                        
                         Connect a PC, with SoMove software and the TeSys island DTM installed, to the service port on the bus coupler using an RJ45 cable.  | 
                     |
| 
                        
                         3  | 
                     
                     
                        
                         Launch the SoMove software on the PC.  | 
                     |
| 
                        
                         4  | 
                     
                     
                        
                         Click the Connect button in the Start screen to establish communication.  | 
                     |