Stall
The Stall function detects high current intensity, typically associated with a locked or stalled motor, while in the Start state.
If enabled, this protection function triggers a Stall trip when the motor is in the Start state, and the maximum phase current exceeds the specified Stall Trip Level for a time longer than the specified Stall Trip Delay.
This function is typically enabled in addition to the Long Start protection function, setting a higher acceptable current intensity level and a shorter trip delay.
Stall Trip Versus Long Start Trip
| 
                                 
                                  D  | 
                              
                              
                                 
                                  Stall Trip  | 
                              
                              
                                 
                                  E  | 
                              
                              
                                 
                                  Stall Level  | 
                              
| 
                                 
                                  F  | 
                              
                              
                                 
                                  Long Start Trip Level  | 
                              
                              
                                 
                                  G  | 
                              
                              
                                 
                                  Long Start Trip Delay  | 
                              
| 
                                 
                                  I  | 
                              
                              
                                 
                                  Current  | 
                              
                              
                                 
                                  Ir  | 
                              
                              
                                 
                                  Rated Current  | 
                              
| 
                                 
                                  t  | 
                              
                              
                                 
                                  Time  | 
                              
                              
                                 
                                  T  | 
                              
                              
                                 
                                  Stall Trip Delay  |