Avatar Settings
  WARNING | 
            
|---|
| 
                  
                   Unintended equipment operation 
                  
 
 Failure to follow these instructions can result in death, serious injury, or equipment
                     damage. 
                   | 
            
Configure the protection functions for each TeSys™ Avatar. Protection functions vary based on the Avatar selected.
Avatar Settings
| 
                        
                         Step  | 
                     
                     
                        
                         Action  | 
                     |
|---|---|---|
| 
                        
                         1  | 
                     
                     
                        
                         Click on the SETTINGS tab in the DTM tool.  | 
                     |
| 
                        
                         2  | 
                     
                     
                        
                         Under AVATARS, click the Avatar to be configured.  | 
                     |
| 
                        
                         3  | 
                     
                     
                        
                         Configure the protection functions for each Avatar.  | 
                     |
| 
                        
                         4  | 
                     
                     
                        
                         Click OK to confirm the settings. Save the project.  | 
                     |
 WARNING