DOCA0270EN-02

I/O Port Assignment

@Updated D2

To access the I/O port assignments for the system, click the I/O Port Assignment tab in the System avatar window. The following information is displayed in the IO Port Assignment view:

  • Avatar Name

  • Input Name/Output Name

  • Device Name

  • Input Number/Output Number

  • Value

  • Fallback Mode

I/O Port Assignment

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?