DOCA0270EN-02

Current Phase Loss

The Current Phase Loss function only applies to three-phase TeSys avatars.

If enabled, then in the motor Start or Run state, this protection function triggers a Current Phase Loss Trip when the current phase unbalance exceeds the Current Phase Loss Trip Level, for a time longer than the Current Phase Loss Trip Delay.

NOTE: The Current Phase Unbalance value is the ratio of the following:
  • The maximum difference between any individual phase RMS current (in absolute value) and the average of the three-phase RMS currents

  • Divided by the average of the three-phase RMS currents

Current Phase Loss Trip

I1

Phase 1 Current

I2

Phase 2 Current

I3

Phase 3 Current

%Iunb

%Current Phase Unbalance

Ialarm

Current Phase Loss Alarm Level

Itrip

Current Phase Loss Trip Level

A

Current Phase Loss Alarm

B

Current Phase Loss Trip

C

Motor Start or Run State

T

Current Phase Loss Trip Delay

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?