Verifying the System Installation in Test Mode
  WARNING | 
            
|---|
| 
                  
                   Unintended equipment operation 
                  Before using the Test mode, ensure that energizing loads
                     will not result in unsafe conditions. 
                  Failure to follow these instructions can result in death, serious injury, or equipment
                     damage. 
                   | 
            
During the pre-operational and operational states you can enter and exit Test mode.
Test Mode allows direct control of the power modules and digital I/O modules using the Operation and Maintenance Tool (OMT). In Test mode, the only TeSys Avatar that is activated is the system avatar . Once you enter Test mode, you must manually exit Test mode to return the TeSys island to the pre-operational state. See Exiting Test Mode.
Verifying the System Installation in Test Mode
| 
                        
                         Step  | 
                     
                     
                        
                         Action  | 
                     
|---|---|
| 
                        
                         1  | 
                     
                     
                        
                         Access the physical devices on the TeSys island : 
  | 
                     
| 
                        
                         2  | 
                     
                     
                        
                         Click the Close or Open command under Test Command.  | 
                     
| 
                        
                         3  | 
                     
                     
                        
                         Click Ok in the WARNING message pop-up window to execute the test command. This will close or open the contactor or input on the device.  | 
                     
| 
                        
                         4  | 
                     
                     
                        
                         Click any device in the TeSys island topology to perform a test command.  | 
                     
| 
                        
                         5  | 
                     
                     
                        
                         After you test all devices, exit Test mode as described in the following table.  | 
                     
Exiting Test Mode
| 
                        
                         Step  | 
                     
                     
                        
                         Action  | 
                     
|---|---|
| 
                        
                         1  | 
                     
                     
                        
                         Click the Diagnostics panel or tab.  | 
                     
| 
                        
                         2  | 
                     
                     
                        
                         Click the Exit Test mode button. A WARNING message pop-up window will appear.  | 
                     
| 
                        
                         3  | 
                     
                     
                        
                         Click Ok in the pop-up window to confirm that you want to exit Test mode. The status banner at the top will indicate that the system is no longer in Test mode.  | 
                     
 WARNING