Avatar Predictive Alarms
Predictive Alarms (PA) alert you of possible events regarding the applications being monitored. Predictive Alarms are triggered by a combination of configured protection functions and PV Input conditions. This section describes the configuration and requirements for the Predictive Alarms function.
The following is the list of avatars with configurable predictive alarms:
- 
                  
                  
Motor One Direction
 - 
                  
                  
Motor Two Directions
 - 
                  
                  
Motor Y/D One Direction
 - 
                  
                  
Motor Y/D Two Directions
 - 
                  
                  
Motor Two Speeds
 - 
                  
                  
Motor Two Speeds Two Directions
 - 
                  
                  
Pump
 - 
                  
                  
Conveyor One Direction
 - 
                  
                  
Conveyor One Direction - SIL Stop, W. Cat 1/2*
 - 
                  
                  
Conveyor Two Directions
 - 
                  
                  
Conveyor Two Directions - SIL Stop, W. Cat 1/2
 
You can set up Predictive Alarms to send a specific message for a protection function without assigning a PV Input condition. PV Input conditions that trigger Predictive Alarms occur when the configured PV Inputs for the avatar are within a selected region of operation based on configurable thresholds. When either the protection function alarm resets or the PV Inputs exit the selected region of operation, the Predictive Alarm resets. Avatars support up to ten Predictive Alarms.
Avatars with Predictive Alarms support the following behavior for the PV Input PA Status output, applying a hysteresis of 5% (rounding down, from the range of valid values).
The following settings are needed to configure Predictive Alarms on avatars with Predictive Alarms support:
- 
                     
                     
Alarm Input
 - 
                     
                     
Alarm Definition