SIL Interface Module Wiring
Using the TeSys island topology and bill of materials, determine the location of the SIL* interface modules (SIMs) on the TeSys island . The SIM is supplied 24 V power and also connects to an external SIL rated device using a spring terminal connector provided with the SIM. Use the following guidelines to complete the 24 V power wiring between the SIL interface modules and the external SIL rated device.
SIM Terminal Block Pinout
| 
                           
                            Pin Number  | 
                        
                        
                           
                            Terminal Identification  | 
                        
                        
                           
                            Signal  | 
                        
|---|---|---|
| 
                           
                            1  | 
                        
                        
                           
                            13  | 
                        
                        
                           
                            MIRROR IN  | 
                        
| 
                           
                            2  | 
                        
                        
                           
                            K1  | 
                        
                        
                           
                            SIL-IN 1  | 
                        
| 
                           
                            3  | 
                        
                        
                           
                            KC  | 
                        
                        
                           
                            SIL COMMON  | 
                        
| 
                           
                            4  | 
                        
                        
                           
                            K2  | 
                        
                        
                           
                            SIL-IN 2  | 
                        
| 
                           
                            5  | 
                        
                        
                           
                            14  | 
                        
                        
                           
                            MIRROR OUT  | 
                        
- 
                  
                  
Remove the spring terminal connector. It is positioned on the top of the module, behind the flat cable connection.
 - 
                  
                  
Using the SIM wiring table, connect 24 V to both K1 and K2 on the removable spring terminal connector, regardless of the control architecture. In wiring category 1 and 2 applications, terminals K1 and K2 must be shorted together. See Accessories Cabling for cable types and sizes.
 - 
                  
                  
Insert the spring terminal connector back into the top of the SIM.