DOCA0270EN-02

Test Mode

In Test mode, the Operation and Maintenance Tool (OMT) can directly control the power modules and the digital I/O modules. You can enter and exit Test mode during the pre-operational and operational states. In Test mode, the only TeSys avatar activated is the System avatar .

NOTE: Once you complete the Test mode activities, you must manually exit Test mode to return the island to the operational state.

To enter Test mode:

  1. Under Test command, click the Close or Open command.

  2. Click OK in the confirmation pop-up window to execute the Test command. This closes or opens the contactor or the device input.

    Execute Test Command Confirmation

  • You can click any device in the island topology and perform a test command.

  • Once you have tested all devices, you must manually exit Test mode.

NOTE: To exit Test mode, see Exit Test Mode.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?