DOCA0270EN-02

Power Outage Events

TeSys island logs the following Power outage events:

  • TeSys island logs power outage events, with a detailed definition of the event description in the bus coupler specifications.

  • Insufficient supply voltage - When this event happen all the modules in TeSys island will not have power supply except bus coupler module. This event will happen when supply voltage is less than 20.7 V.

  • Insufficient supply on close command to starters.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?