Trip Reset Command
NOTE: The Reset function may lead to immediate energizing of the load, with an active command from the PLC or the Force mode function.
![]() |
---|
UNINTENDED EQUIPMENT OPERATION
Before resetting the protection functions, verify that
this function does not result in unsafe conditions.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
A tripped TeSys avatar can only reset protection trips after receiving a Trip Reset command and if all the trip reset conditions are met for all its protection functions. This mechanism helps ensure that, after a trip, normal operation can only resume when all the defined normal operational conditions are met again.
When a protection function has caused an avatar to trip, the avatar remains in the tripped state until both of the following occur:
-
The operational conditions again match the trip reset conditions of the protection function
-
The avatar receives a Trip Reset command
The Trip Reset command applies to all the protection functions enabled for a given avatar. However:
-
The Tripped state output is set to false only for those protection functions whose trip reset conditions are met.
-
The Tripped status output remains set to true for those protection functions whose trip reset conditions are still not met.
A tripped avatar has at least one tripped protection function (with a Tripped status set to true).
According to the same logic, an avatar that is not tripped has no tripped protection functions (no protection with a Tripped status set to true).
Tripped protection functions can be reset by the Auto-Reset function, via the controller or by using one of the digital tools.
The following table describes the Trip Reset Conditions, including hysteresis, for all avatars.
Trip reset conditions
Protection function |
Trip reset conditions |
---|---|
Thermal Overload |
Thermal capacity has decreased below Thermal Reset Threshold (no hysteresis). |
Motor Overheat |
Motor temperature has decreased below Motor Overheat Reset Threshold (no hysteresis). |
Current Phase Unbalance |
Current unbalance has decreased below Current Phase Unbalance Trip Level. |
Current Phase Loss |
Current unbalance has decreased below Current Phase Loss Trip Level. |
Jam |
Maximum phase current has decreased below Jam Trip Level. |
Undercurrent |
Average current has increased above Undercurrent Trip Level. |
Long Start |
Average current has decreased below 30% Ir (no hysteresis). |
Overcurrent |
Maximum phase current has decreased below Overcurrent Trip Level. |
Stall |
Maximum phase current has decreased below Stall Trip Level. |
Ground Current |
Ground current has decreased below Ground Current Trip Level. |
Current Phase Reversal |
Average current has decreased below 30% Ir (no hysteresis). |
Phase Configuration |
Average current has decreased below 30% Ir (no hysteresis). |
Where indicated, protection functions apply a 5% hysteresis value to the trip reset conditions. This increases the stability of the protection functions’ behavior. The trip reset is only authorized when normal conditions and this extra 5% margin are recovered.
For instance, the Jam protection function triggers a trip when the maximum phase current exceeds the defined Jam trip level. The trip reset conditions are met when the maximum phase current decreases below the Jam trip level minus 5%.
Additionally, setting the Trip Enable parameter for a protection function to Disable meets the Trip reset condition for that protection function.