DOCA0270EN-02

Connecting with TeSys™ island DTM

You can connect to the TeSys island using the default IPv4 IP address on the bus coupler with SoMove software running the TeSys island DTM. The PC must be on the same subnet as the default IPv4 address of the bus coupler. The TeSys island default addressing mode is DHCP. While in DHCP mode, the island can be reached with a default IP address of 10.10.0.1 with subnet mask 255.0.0.0.

Proceed to the Connecting to TeSys island with SoMove Software procedure to use the TeSys island DTM.

If you prefer to connect to the TeSys island using the OMT, proceed to the Connecting with the OMT procedure.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?