DOCA0270EN-02

Status

To access the status information for the system, click the Status tab in the System avatar window. The following information is displayed in Status view:

  • System status

  • Alarm message

  • Force mode status

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?