Installing the LAD9R3 Kit (40–65 A Starters)
The accessories in the LAD9R3 kit are used to join adjacent 40–65 A (size 3) starters in two speed or two direction Avatars. To install the accessories, perform the steps in the following table and refer to Installing the LAD9R3 Assembly Kit.
LAD9R3 Installation Procedure
| 
                           
                            Step  | 
                        
                        
                           
                            Action  | 
                        
|---|---|
| 
                           
                            1  | 
                        
                        
                           
                            Push the Everlink™ terminals toward you to remove them from the starter.  | 
                        
| 
                           
                            2  | 
                        
                        
                           
                            On the starter on the left, remove the small pieces of plastic located at the top and the bottom on the right side of the starter. Do not remove these pieces from the left side of the starter.  | 
                        
| 
                           
                            On the starter on the right, remove the small pieces of plastic located at the top and the bottom on the left side of the starter. Do not remove these pieces from the right side of the starter.  | 
                        |
| 
                           
                            3  | 
                        
                        
                           
                            Install the LAD4CM mechanical interlock onto the starter on the right. Make sure the blue clip goes into the side of the starter. The spring-loaded clip will attach it to the side of the starter. You will hear a click once the connection is made.  | 
                        
| 
                           
                            4  | 
                        
                        
                           
                            Attach the starter on the left to the mechanical interlock. You will hear a click once the connection is made.  | 
                        
| 
                           
                            5  | 
                        
                        
                           
                            Install the LA9D65A6 parallel link at the top of the starters.  | 
                        
| 
                           
                            Install the LA9D65A69 reversing link at the bottom of the starters.  | 
                        |
| 
                           
                            6  | 
                        
                        
                           
                            Slide the Everlink terminals on the bottom and top of the starters. Push the Everlink terminal towards the starter until you hear a click.  | 
                        
To separate the starters and remove the accessories, perform the steps in the following table and refer to Removing the LAD9R3 Assembly Kit.
LAD9R3 Removal Procedure
| 
                           
                            Step  | 
                        
                        
                           
                            Action  | 
                        
|---|---|
| 
                           
                            1  | 
                        
                        
                           
                            Completely loosen the screws on the Everlink terminals. Push the Everlink terminals toward you to remove them from the starter.  | 
                        
| 
                           
                            2  | 
                        
                        
                           
                            Remove the reversing link from the bottom of the starters.  | 
                        
| 
                           
                            3  | 
                        
                        
                           
                            Remove the parallel link from the top of the starters.  | 
                        
| 
                           
                            4  | 
                        
                        
                           
                            Use a flat-head screwdriver to lift the blue actuator on the top and bottom of the mechanical interlock installed between the two starters.  | 
                        
| 
                           
                            5  | 
                        
                        
                           
                            Remove the mechanical interlock.  |