DOCA0270EN-02

Motor Overheat

The Motor Overheat function is only available for TeSys avatars whose Temperature Sensor Available parameter is activated. These avatars include an analog I/O module, which is wired to the temperature input from the temperature sensor associated with the protected motor.

If enabled, this protection function performs the following:

  • Signals a Motor Overheat Alarm when the motor temperature exceeds the Motor Overheat Alarm Level

  • Triggers a Motor Overheat Trip when the motor temperature exceeds the Motor Overheat Trip Level, for a time longer than the Motor Overheat Trip Delay

The Motor Overheat Trip Reset Threshold parameter sets the percentage below which the temperature must fall, before a trip reset is allowed.

Motor Overheat Trip and Alarm

A

Motor Temperature

B

Motor Temperature ≥ Motor Overheat Alarm Level

C

Motor Temperature ≥ Motor Overheat Trip Level

D

Alarm

E

Trip

T

Motor Overheat Trip Delay

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?