Current Phase Unbalance
The Current Phase Unbalance function only applies to three-phase TeSys avatars.
If enabled, this protection function performs the following:
- 
                  
                  
Signals a Current Phase Unbalance Alarm when the current phase unbalance exceeds the specified Current Phase Unbalance Alarm Level
 - 
                  
                  
Triggers a Current Phase Unbalance Trip when the current phase unbalance exceeds the specified Current Phase Unbalance Trip Level for a time longer than the specified Current Phase Unbalance Trip Delay
NOTE: Separate trip delays are configurable for Run State and Start State. 
| 
                           
                            I1  | 
                        
                        
                           
                            Phase 1 Current  | 
                        
                        
                           
                            I2  | 
                        
                        
                           
                            Phase 2 Current  | 
                        
| 
                           
                            I3  | 
                        
                        
                           
                            Phase 3 Current  | 
                        
                        
                           
                            %Iunb  | 
                        
                        
                           
                            %Current Phase Unbalance  | 
                        
| 
                           
                            Ialarm  | 
                        
                        
                           
                            Current Phase Unbalance Alarm Level  | 
                        
                        
                           
                            Itrip  | 
                        
                        
                           
                            Current Phase Unbalance Trip Level  | 
                        
| 
                           
                            T1  | 
                        
                        
                           
                            Current Phase Unbalance Trip Delay—Start  | 
                        
                        
                           
                            T2  | 
                        
                        
                           
                            Current Phase Unbalance Trip Delay—Run  | 
                        
| 
                           
                            A  | 
                        
                        
                           
                            Motor Start State  | 
                        
                        
                           
                            B  | 
                        
                        
                           
                            Motor Run State  | 
                        
| 
                           
                            C  | 
                        
                        
                           
                            Current Phase Unbalance Alarm  | 
                        
                        
                           
                            D  | 
                        
                        
                           
                            Current Phase Unbalance Trip  | 
                        
- 
                     
                     
The maximum difference between any individual phase RMS current (in absolute value) and the average of the three-phase RMS currents
 - 
                     
                     
Divided by the average of the three-phase RMS currents