DOCA0270EN-02

Powering On the island

To power on the island:

  1. Energize the bus coupler with 24 V.

    The island enters the pre-operational stage. Once it finishes booting and all settings have been applied, the island enters the operational state.

    NOTE: You can enter and exit Test mode using the digital tools throughout the pre-operational and operational states.
  2. Verify that the PWR LED is illuminated and shows a steady green, indicating that power is applied and the island is operational.

EtherNet/IP™ Bus Coupler

 

PROFINET® Bus Coupler

 

PROFIBUS® Bus Coupler

   
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?