SIL Starters
  WARNING | 
            
|---|
| 
                  
                   UNINTENDED EQUIPMENT OPERATION 
                  For complete instructions about functional safety, refer
                     to the TeSys™ island Functional Safety Guide, 8536IB1904. 
                  Failure to follow these instructions can result in death, serious injury, or equipment
                     damage. 
                   | 
            
SIL* starters provide similar functions to standard starters but are associated with a SIL interface module.
The main functions of the SIL starters are as follows:
- 
                  
                  
Provide Stop Category 0 and Stop Category 1* functionality
 - 
                  
                  
Provide operational control for loads
 - 
                  
                  
Measure electrical data related to the load
 - 
                  
                  
Provide energy monitoring data when a voltage interface module is installed in the TeSys island
 
Multiple SIL starters might be needed for a single TeSys avatar function. For example, the avatar Motor Two Directions - SIL Stop, W. Cat 1/2* includes two SIL starters. In addition, avatars using SIL starters always include a SIL interface module.
The SIL starters are connected:
- 
                  
                  
Upstream to a circuit breaker
 - 
                  
                  
Downstream to the load
 
The SIL starters communicate with the bus coupler, sending operational data and receiving commands.
SIL Starter Ratings
| 
                        
                         Power Ratings  | 
                     
                     
                        
                         Amperage  | 
                     
                     
                        
                         Reference  | 
                     |
|---|---|---|---|
| 
                        
                         kW  | 
                     
                     
                        
                         hp  | 
                     ||
| 
                        
                         4  | 
                     
                     
                        
                         5  | 
                     
                     
                        
                         0.18–9  | 
                     
                     
                        
                         TPRSS009  | 
                     
| 
                        
                         11  | 
                     
                     
                        
                         15  | 
                     
                     
                        
                         0.5–25  | 
                     
                     
                        
                         TPRSS025  | 
                     
| 
                        
                         18.5  | 
                     
                     
                        
                         20  | 
                     
                     
                        
                         0.76–38  | 
                     
                     
                        
                         TPRSS038  | 
                     
| 
                        
                         30  | 
                     
                     
                        
                         40  | 
                     
                     
                        
                         3.25–65  | 
                     
                     
                        
                         TPRSS065  | 
                     
| 
                        
                         37  | 
                     
                     
                        
                         40  | 
                     
                     
                        
                         4–80  | 
                     
                     
                        
                         TPRSS080  | 
                     
 WARNING