DOCA0270EN-02

Physically Locate

Before starting any activities using the OMT, verify that you are connected to the correct TeSys island .

Perform the following steps:

  1. Click the Control Panel icon.

  2. Click Physically Locate.

    Result: The bus coupler’s PWR LED illuminates a steady yellow for 5 s to help you identify which device the OMT is communicating with.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?