DOCA0270EN-02

System Security

To modify the security settings for the system:

  1. In the Admin Options panel, click the arrow to expand the Security Settings section.

  2. Change the settings you wish to modify.

  3. Click Save.

Security Settings

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?