DOCA0270EN-02

System Logs

TeSys island maintains two log files:

  • System event log related to the normal operation of the system

  • Security related audit log

Multiple events occurring simultaneously (for example, alarms that are simultaneously cleared when the load is turned off) are logged as individual events. There is no constraint or preference for the order in which multiple simultaneous events are logged.

To view the system logs:

  1. Click the User Management panel.

  2. Expand the System Logs window.

You can download the current version of the Event log or the Audit log.

  • The event log is a .csv file containing the events used for debugging.

  • The audit log is a cybersecurity feature showing actions related to user login, user access to force mode, and user downloads of new context files. It logs any security related event.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?