Groups
Each user is assigned to a group that defines the user’s privileges for read and write access. Click Learn More in the User Management section to open the Access Management window. This window displays the available groups, and allows the administrator to select which panels and functions the group can access. See the figure below.
From the drop-down menus for each type of user, select which rights to assign for that panel. The options are:
- 
                  
                  
None
 - 
                  
                  
Limited
 - 
                  
                  
Full
 
You can select the options for the different types of user:
- 
                  
                  
Administrator
 - 
                  
                  
Automation Engineer
 - 
                  
                  
Maintenance Level 1
 - 
                  
                  
Maintenance Level 2
 - 
                  
                  
Operator
 
When all selections are complete, click the X in the top left of the Access Management window to close it.