DOCA0270EN-02

Installing Standard Starters and SIL Starters

NOTE: Safety Integrity Level according to standard IEC 61508.

This section contains instructions for joining adjacent starters with assembly accessories for use in two direction, two speed, and wye-delta (Y/D) Avatars. It also describes how to install the starters on DIN rail. Remove power before performing the steps in this section. Read and understand the information in Precautions before performing any procedures in this guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?