System Event Log Attributes
System Event Log attributes are defined in the following table.
| 
                        
                         Attribute  | 
                     
                     
                        
                         Description  | 
                     
|---|---|
| 
                        
                         timestamp  | 
                     
                     
                        
                         The system time YYYY-MM-DDThh:mm:ss.mmm Example: 2018-01-02T15:02:59.970  | 
                     
| 
                        
                         avatarName  | 
                     
                     
                        
                         The user defined avatar name  | 
                     
| 
                        
                         avatarNumber  | 
                     
                     
                        
                         The number of the avatar in the digital tool  | 
                     
| 
                        
                         avatarSILGroup  | 
                     
                     
                        
                         The SIL* group of the avatar  | 
                     
| 
                        
                         deviceTag  | 
                     
                     
                        
                         The user defined device tag  | 
                     
| 
                        
                         deviceNumber  | 
                     
                     
                        
                         The number of the device in the physical order of the system (the Node ID on the internal bus)  | 
                     
| 
                        
                         value  | 
                     
                     
                        
                         The new value of the data change event being logged.  |