SIL Interface Module (SIM)
Device Status is the top LED on all TeSys island modules except the bus coupler.
Device Status LED
|
Indicator State |
Summary |
Description |
|---|---|---|
|
Single Flash Green/Red |
LED Diagnostic |
Visual indication that LEDs are operational. |
|
Steady Off |
Off |
Module not energized. |
|
Steady Red |
Device Major Event |
Internal device event. |
|
Flashing Red |
Not Ready |
Discovery, addressing, firmware update, Device Minor Event, etc. |
|
Steady Green |
Ready |
Module is ready. |
SIL Status LED
|
Indicator State |
Description |
|---|---|
|
Single Flash Green/Red |
Visual indication that LEDs are operational. |
|
Steady Off |
Module not energized or not ready. |
|
Steady Green |
No SIL Group Stop command. |
|
Flashing Green |
Successful SIL Group Stop command, not yet in SIL Stop State. |
|
Flashing Red |
Successful SIL Group Stop command, but indicative of a wiring issue. SIL Stop State achieved. |
|
Steady Red |
Successful SIL Group Stop command. SIL Stop State achieved. |