Units
To change the units of measurement displayed in the OMT, perform the following steps:
- 
                  
                  
In the USER PREFERENCES window, click UNITS.
 - 
                  
                  
Change the settings as desired. For more information about the settings, refer the following table.
OMT settings for units of measurement
Unit
Options
Impacts
Motor Power
kW, hp
- 
                                       
                                       
Instantaneous Total Active Power
 - 
                                       
                                       
Maximum Total Active Power
 
Temperature
°C, °F
- 
                                       
                                       
Motor Overheat chart - Trip Status
 - 
                                       
                                       
Motor Overheat options - Thermal Protection settings
 
Date
dd/mm/yyyy, mm/dd/yyyy
- 
                                       
                                       
Banner time display
 - 
                                       
                                       
Log displays
 - 
                                       
                                       
Trip registers
 - 
                                       
                                       
Timestamp values for energy, power and voltage monitoring
 
 - 
                                       
                                       
 - 
                  
                  
Click Save.