DOCA0270EN-02

Mounting the I/O and Interface Modules on DIN Rail

This section covers installation of:

  • Digital I/O Modules

  • Analog I/O Modules

  • SIL* Interface Modules (SIM)

  • Voltage Interface Modules (VIM)

Before installing modules on the TeSys island , refer to the TeSys island topology to ensure you are installing them in the correct sequence.

To install a module on DIN rail, position the top groove of the module onto the top edge of the DIN rail and press it against the rail until you hear the clip snap into place. See the figure below.

I/O Modules (TPRDG4X2 and TPRAN2X1) and Interface Modules (TPRSM001 and TPRVM001) (mm/in.)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?