DOCA0270EN-02

Conveyor Avatars

There are four conveyor application avatars , which include the following:

  • Standard or SIL* starter modules

  • One or more digital I/O modules for PV switches and local control inputs

  • One or more analog I/O modules for PV inputs and motor temperature monitoring, if enabled

  • Configurable control logic

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?